Wireless Charging solution Wiki
This Topic is used for Wireless Charging solution 1.Mcu C drive code: GitHub - STMicroelectronics/STWirelessCharging-C-Drivers: Standard C platform-independent drivers for wireless charging ICs
This Topic is used for Wireless Charging solution 1.Mcu C drive code: GitHub - STMicroelectronics/STWirelessCharging-C-Drivers: Standard C platform-independent drivers for wireless charging ICs
Hello ST Community,I am currently developing a product using the PM8805 chip and have purchased and tested the STEVAL-POE001V1 evaluation board. Based on the reference design provided by ST, I created my own circuit diagram and manufactured a custom ...
I want to use the PM8805 as POE controller in a custom project for a 25W classified POE device. The PM8805 should generate the input power for 2 boards in this device.However, when connecting only one board with approx. 30uF input capacitance, the po...
Hello,I'm planning to use the STGAP3SXS Gate driver on SiC MOSFETS SCT040W120G3AG by ST.I want to know if there is an available Spice models for this part as I want to simulate their behaviorThank You!.
I'm working on developing product, for that I was going through the documents of AC/DC & DC/DC products for reference but, I'm not able to find any detailed documents. If you have any application notes or design documents regarding these products, it...
I am using STWBC2-HP and STWLC99 for development. The output voltage at the receiver end is set to 10V, and the current limit at the transmitter end is set to 5A. However, the actual current at the transmitter end can only reach a maximum of 0.8A, an...
Hi I am developing new carrier board for COMe type-6 Module. Where i have a requirement of Display port to connect an external display with 5v @3A max, 9V@1.67A max. below block diagram has 1. COMe type 6 module (Host).2. Re-driver (MPN: TUSB1046A-D...
Hello ST Team, Greeting from Uniglobus, is the child R&D Electronics company of Polycab India limited My self Grishma Bhatt, I am Power Electronics Design Engineer We would like to start a new product 3.3KVA Single phase non isolated solar on grid In...
Can the IPS2050H withstand a full short circuit on the outputs?Let's say the IPS2050H output is connected to a board power connector. What happens if:1. The connector is first short circuited and then the IPS2050H is turned on.2. The IPS2050H is alre...
Hi Sir, Does the STUSB1602 support Alternate Mode? Is an MCU required to enable it, or can it be implemented directly with the MCU alone? Is there any example code available? Thank you.
Hi the datasheet does not contain the thermal junction temperatures for the VFQFPN48, hence hard to work out the max thermal temps for the device. please can you supplyregardsRoss