Product overview
Description
STMCube™ is an STMicroelectronics original initiative to make developers' lives easier by reducing development effort, time and cost. STM32Cube is the implementation of STMCube that covers the whole STM32 portfolio.
STM32Cube includes STM32CubeMX, a graphical software configuration tool that allows the generation of C initialization code using graphical wizards.
It also comprises the STM32CubeL1 MCU Package composed of the STM32Cube hardware abstraction layer (HAL) and the low-layer (LL) APIs, plus a consistent set of middleware components (RTOS, USB, FAT file system, Graphics and STM32 touch sensing). All embedded software utilities are delivered with a full set of examples running on STMicroelectronics boards.
The STM32Cube HAL is an STM32 embedded software layer that ensures maximized portability across the STM32 portfolio, while the LL APIs make up a fast, light-weight, expert-oriented layer which is closer to the hardware than the HAL. HAL and LL APIs can be used simultaneously with a few restrictions.
Both the HAL and LL APIs are production-ready and have been developed in compliance with MISRA C®:2004 guidelines with some documented exceptions (reports available on demand) and ISO/TS 16949. Furthermore, ST-specific validation processes add a deeper-level qualification.
STM32CubeL1 gathers in one single package all the generic embedded software components required to develop an application on STM32L1 microcontrollers. Following STM32Cube initiative, this set of components is highly portable, not only within STM32L1 Series but also to other STM32 Series. In addition, the low-layer APIs provide an alternative, high-performance, low-footprint solution to the STM32CubeL1 HAL at the cost of portability and simplicity.
HAL and LL APIs are available under open-source BSD license for user convenience.
-
All features
- Consistent and complete embedded software offer that frees the user from dependency issues
- Maximized portability between all STM32 Series supported by STM32Cube
- More than 90 examples for easy understanding
- High quality HAL and low-layer API drivers using CodeSonar® static analysis tool
- STM32L1-dedicated middleware including USB Host and Device, FAT file system, RTOS, Graphics and touch sensing library
- Free user-friendly license terms
- Update mechanism that can be enabled by the user to be notified of new releases
Get Software
Part Number | General Description | Latest version | Supplier | ECCN (EU) | ECCN (US) | Download | All versions | |
---|---|---|---|---|---|---|---|---|
Patch_CubeL1 | Patch for STM32CubeL1 | 1.10.5 | ST | NEC | EAR99 | Get latest | ||
STM32CubeL1 | STM32Cube MCU Package for STM32L1 series | 1.10.0 | ST | NEC | 3D991 | Get latest |
Featured Videos
In our continued efforts to simplify developers’ life within the STM32Cube environment, we just introduced a new video demonstrating how to easily port an example built using ST’s new STM32Cube Low-Layer APIs from one board (NUCLEO-L476RG) to another (32L496GDISCOVERY) within the same STM32 family.