Current sense amplifiers
A current sense amplifier is a differential amplifier providing an analog output voltage proportional to the current flowing into a load connected on its input.

ST's current sense amplifier IC portfolio offers a large variety of high-performance devices.

Current sensing solutions add valuable safety and protection features to system designs. They provide information to control current in power systems and avoid overheating and short circuits. Current sensing is also an essential part of energy metering to ensure power-efficiency and minimize environmental impact.
Key features
The main features of ST's portfolio of current sensing ICs ensure robustness and application safety:
High-voltage
Tolerance to high voltage ranges and protection mechanisms to handle negative voltage are essential in high-power systems such as batteries in electric vehicles. Our current sense amplifiers can work in high voltage applications avoiding additional external protections components and simplifying the final schematic.
Precision / high-accuracy
Using a precision current sense amplifier allows designers to measure small voltage drops across shunt resistors with minimal error. Small shunt resistors values are necessary to minimize the power dissipation. Thanks to highly accurate current measurements, precision current sense amplifiers offer a better efficiency and thermal performance.
What are the main benefits of a current sense amplifier?
Current sense amplifiers provide several benefits for designers, including the possibility to:
- measure current ranging from a few milli amperes to several hundreds
- perform real-time current measurement in several topologies
- precisely measure current, thanks to an integrated matched resistive gain network
- reduce PCB size thanks to integrated gain resistance
- sustain extended input common mode voltage, far beyond the power supply rail
How does a current sense amplifier work?

The working principle of a current sensing amplifier is based on Ohm's law. When load current flows through a shunt resistor (Rshunt) present on inputs, it generates a voltage drop called VSENSE. This voltage is generally small to limit power dissipation losses.
VSENSE is then amplified with an internal instrumentation amplifier. The resulting output voltage (VOUT) is a voltage which is proportional to the Ioad current. It can then be processed with an ADC (analog-to-digital converter).
What are the main types of current sense amplifiers?

High-side amplifiers
The current is measured between the supply rail and the load. The DC voltage applied on the input pins can be much higher than the power supply.
Benefits
- Short-to-ground fault detection
- High immunity against ground disturbance
- Current monitored directly from the source
Challenges
- High-input common-mode voltages
- Support fast variation of input common mode voltage
Low-side amplifiers
The current is measured between the load and the ground. The voltage applied on the input pins is close to the ground.
Benefits
- Simple implementation
- Cost-effective solution
- VICM (input common-mode voltage) close to GND (zero-voltage point)
Challenges
- Difficult to detect short-cut to ground
- Multiple output power supply (all current are combined in GND line)
- May disturb the ground voltage seen by the load
Bi-directional VS unidirectional
In some applications, the current can flow into the load in both directions. This is the case for motor control applications used in H-Bridge topologies. In this case, the current sense amplifier must have one additional pin, called VREF. The VREF pin allows designers to set the output reference anywhere within the power supply range. A bidirectional amplifiers can be used as a unidirectional current sense amplifier, setting the reference to one voltage rail.
How to choose the right current sense amplifier for your design?
-
Define the configuration required for your device
High-side configuration: Select the current sense amplifier depending of the max common mode voltage (VICM) required by the application and its power supply (VCC).
Low-side configuration: Select a current sense amplifier that can work with a common mode voltage close to 0 volts.
Operational amplifiers can be also used, adding 4 external resistors to set the gain. However, the size of the PCB will be larger and accuracy can be lower. -
Look into the direction of current flows
After defining the configuration required, ask yourself if the current in your application needs to flow in both directions, in order to choose a bidirectional or unidirectional current sensing.
-
If accurate measurements are needed
Several parameters related to the application must be taken into account. Depending on the current range to be measured and the shunt resistor used, the voltage drop into the shunt resistor can be very small (hundreds of µV). For better accuracy, it is important to consider the error related to offset and accuracy gain.
Featured Videos
Recommended for you
Low/high-side bidirectional current sense amplifiers for industrial and automotive applications
Based on a zero-drift architecture that delivers high performance for precision current sensing, the TSC21x family brings excellent accuracy and robustness to your design.
TSC21x products are available in six different versions (TSC210 / TSC211 / TSC212 / TSC213 / TSC214 / TSC215), offering different gain. They can operate over a broad supply voltage range, from 2.7 to 26 V, and support temperatures ranging from -40 to 125 °C, making them ideal for industrial and automotive applications.
Evaluation board is also available, to support developers in their designs
Bidirectional low-side current sensing amplifier for automotive and industrial applications
The TSC1801 is a precision low-side current measurement amplifier designed to sense voltage drops across shunt resistors at low common-mode voltages.
With a fixed gain of 20 V/V, it ensures accurate and high-bandwidth current sensing for applications like low-side motor control and power management in Solar Powered Systems, HEV and EV.
Low- and high-side current sense amplifiers with overcurrent protection for automotive, industrial, and telecom applications

The TSC200, TSC201, and TSC202 are current sense amplifiers delivering an analog voltage output, designed for both high- and low-side sensing.
The devices can detect current through a shunt resistor across -20 V to +80 V of common-mode voltage, featuring an amplification gain of 20 V/V for TSC200, 50 V/V for TSC201, and 100 V/V for TSC202.
AEC-Q100 qualified, the TSC200, TSC201, and TSC202 integrate an open-drain comparator with an output latch function and an internal 0.6 V voltage reference connected to the input.
To support developers in their designs is available the STEVAL-AETKT3V1 evaluation kit.
The ultimate solution for high voltage (100 V) precision current sensing in Automotive and Industrial applications
AEC-Q100 automotive qualified and packaged in both standard SO-8 and MiniSO-8, the TSC2020, TSC2021, and TSC2022 are designed to sense very low drop voltages, resulting so the perfect choice for precision current measurement, overcurrent protection, current monitoring, and feedback loops.
With advanced bidirectional sensing capabilities and available in three fixed gain version, x20 V/V (TSC2020), x50 V/V (TSC2021), x100 V/V (TSC2022), the devices can accurately sense currents up to 100 V common mode voltage via a shunt resistor.
The STEVAL-AETK41V1 evaluation kit is available to support engineers in their design.
High-voltage, bidirectional current-sense amplifiers
Able to sense very low drop voltages as low as 10 mV, our TSC2010 (20 V/V Gain), TSC2011 (60 V/V) and TSC2012 (100 V/V) high-voltage bidirectional current sense amplifiers (available both as Automotive and Industrial grade) can sense the current thanks to a shunt resistor over a wide range of common mode voltages from –20 to + 70 V, regardless of the supply voltage. Available also with extended temperature range (-40 to 150 °C) : TSC2010H, TSC2011H and TSC2012H.
An Evaluation board can be ordered (STEVAL-AETKT1V2), to support developers in their designs.