ARM TechCon 2019
Website: Click here
Visit us at: Booth 843
ARM TechCon 2019
San Jose Convention Center
Santa Clara, California
October 8-10, 2019
Expo Hall Hours: | Conference Hours: | |
Wednesday, October 9 | 11:30 am – 6:30 pm Thursday, October 10 | 11:30 am – 6:00 pm | Tuesday, October 8 | 8:30 am – 6:00 pm Wednesday, October 9 | 8:30 am – 6:30 pm Thursday, October 10 | 8:30 am – 5:30 pm |
Meet with our experts at booth # 843 to learn about innovative ST technologies that are enabling a smarter, richer, greener and more enjoyable world.
STMicroelectronics Featured Products include:
STM32MP1 - Multi-Core Processor
General purpose multicore microprocessor with flexible architecture including high-performance and real time cores for Industrial, Consumer, Medical and Smart Home applications.
STM32Cube.AI on STM32H7 and STM32L5
Visual food classification demonstrator using the new dual core STM32H7 along with the STM32Cube.AI Artificial Intelligence extension to the STM32CubeMX tool.
Advanced User Interface with TouchGFX and STM32
NFC Sensor Tag form factor reference design with Cloud connectivity offers a simple and cost-effective implementation for integrating the antenna into your application: application notes, reference designs, antenna computation tools, e-presentations and e-learning.
Spend the afternoon with us during our hands-on STM32 educational workshop at its NEW location - the San Jose Convention Center on Wednesday, October 8:
STM32 G4 Mixed Signal Microcontroller Hands-on Workshop:
Wednesday, October 9 | 2:30pm - 5:30 PM | Room 220B
The new STM32G4 mixed signal MCU is ideal for todays advanced control and measurement applications such as three-phase brushless motor control, instrumentation and digital switch-mode power supplies with its rich set of analog peripherals, mathematical accelerators and high resolution timers. This one-day hands-on workshop will introduce embedded engineers to the new STM32G4 features through hands-on exercises. The hands-on exercises will be on the STM32G474 Discovery board that features the STM32G474RET6 MCU based on Arm® Cortex®-M4 core operating up to 170MHz with 512 Kbytes of Flash memory, 128 Kbytes of SRAM in a LQFP64 package along with several application circuits including a digital power buck-boost converter and RGB power LED.
You will learn:
- The new features and peripherals on the STM32G4 microcontroller series
- How to get started with the STM32G474 Discovery kit (B-G474E-DPOW1), STM32CubeMX and Keil MDK
- How to configure and use the new features of the STM32G4 through hands-on exercises
You will need a laptop with type A USB port and Type C USB port and administrator rights running Windows 7 or later, or a MacBook running Windows (Parallels, VM Fusion, etc.), with a minimum 2 GHz processor, 4 GBs of RAM and 10 GBs of free disk space. For laptop with only USB Type C ports, please bring a Type A (Female to Type C (Male) adapter. ST will provide the development kit and all software.
ST will provide the required STM32G474 Discovery kit and software. SPACE IS LIMITED FOR THIS SESSION – FIRST COME, FIRST SEATED. Must be present with your laptop and stay for training to receive free kit.
For more information and to register directly for Arm TechCon 2019 visit https://www.armtechcon.com/.