Expanding Bluetooth® LE capabilities using Coded PHY and Extended Advertisement
![]() | Learn to use Bluetooth® LE 5.0 Coded PHY for long-range applications and Advertising Extension for larger beacon payloadsVirtual hands-on workshop with live tech support |
Please join us for a free online workshop to learn how to expand Bluetooth LE capabilities with Coded PHY and Extended Advertisement using ST's new BlueNRG-LP Bluetooth Low Energy 5.2 certified System-on-Chip (SoC) and associated hardware evaluation platform and software development kit.
In today’s world Bluetooth-enabled IoT applications are becoming more and more demanding, not only in terms of the power consumption but also regarding range capabilities and the quantity of data being advertised – especially in beacon applications.
ST’s BlueNRG-LP is a Bluetooth LE 5.2 certified SoC that helps designers meet these demands not only with its ultra-low power consumption and best-in-class radio performance, but also by supporting Bluetooth 5.0 Coded PHY, which increases the range of a Bluetooth LE 5.0-enabled device up to 4x. And with the Advertisement Extension feature, the amount of data that a Bluetooth LE 5.0 device can advertise is increased by 8x.
This workshop is self-paced and can be accessed on-demand any time after the start of the selected session (see Session dates and times). Please note that live tech support via break-out rooms will be available only during the scheduled session hours.
Participation details
This workshop is open to Americas residents only.
Two STEVAL-IDB011V1 kits are required to participate in the workshop exercises. The STEVAL-IDB011V1 is an evaluation platform designed to help you develop and test Bluetooth low energy applications using the BlueNRG-LP SoC. Exclusively for attendees of this workshop, a limited number of the kits will be available on a buy one, get one free basis for a price of $67.38 USD (total for both components). You will receive purchase instructions by email soon after we receive your request to participate.
You will need to complete the purchase of these discounted kits in order to be confirmed for a workshop session.
What you will learn
This hands-on workshop will introduce you to Bluetooth LE 5.0 Coded PHY and Advertisement Extension features, including:
- The theory behind Bluetooth LE's Coded PHY feature
- How to configure and test Bluetooth LE's Coded PHY using the STEVAL-IDB011V1
- The theory behind Bluetooth LE's Advertisement Extension feature
- How to configure and test Bluetooth LE's Advertisement Extension using the STEVAL-IDB011V1
Prerequisites
This hands-on workshop is a working session and requires a computer running the 64-bit version of Windows® 10. Administrator rights are needed for software and driver installation. Two STEVAL-IDB011V1 kits are required for this workshop.
The use of two screens is recommended so that you can watch, pause, and rewind the instruction video on one screen while completing the workshop on the other.
Session dates and times
Date | Time | Location | Status | |
Session 1 | Tuesday, 05 Oct 2021 | 1:00 pm - 4:00 pm ET | Online | Full |
Session 2 | Thursday, 07 Oct 2021 | 1:00 pm - 4:00 pm ET | Online | Full |
Session 3 | Wednesday, 13 Oct 2021 | 1:00 pm - 4:00 pm ET | Online | Full |
Meet your instructors
![]() | Josh Hogan Josh is a Product Marketing Engineer at STMicroelectronics focusing on General Purpose Analog and RF products. Based in Burlington, MA, he joined ST in 2020 following internships as a test engineer at Johnson Controls and software engineer at NEC Energy Solutions. Josh received his BS in Electrical & Computer Engineering from Worcester Polytechnic Institute in 2020. |
![]() | Julio Sanchez Julio is a Product Marketing Engineer for STMicroelectronics’ RF business unit in the Americas, a position he has held since 2017. Julio began his career in 2005, working for several companies as an FAE before joining ST Mexico in 2015 as a Sr. Key Account Manager. Based in Irvine, CA, Julio holds a degree in Electronics and Communications and a Master’s in Embedded Systems. |
![]() | José Ricardo de Freitas Ricardo is a Senior Engineer at STMicroelectronics and is responsible for Power Line Communications products in the Americas region. He holds a Bachelor's in Electrical Engineering from the Maua Engineering School and an MBA in Business Administration from FGV. |
About the hardware and software tools used in the workshop
The STEVAL-IDB011V1 evaluation platform features the BlueNRG-LP which is an ultra low power consumption Bluetooth LE 5.2 certified SoC with best-in-class radio performance, in combination with inertial and environmental MEMS sensors, a digital MEMS microphone, and various interface buttons and LEDs.
The STSW-BNRGLP-DK software development kit provides a Bluetooth low energy binary library with a complete set of APIs to access the Bluetooth low energy functionality offered by the BlueNRG-LP SoC. The software development kit also provides a set of Bluetooth low energy demonstration applications supporting typical Bluetooth low energy use cases. Each demo application comes with a complete set of headers and source files.