ISSCC 2021 International Solid-State Circuits Virtual Conference
2021 International Solid-State Circuits Virtual ConferenceFebruary 13 - 22, 2021 Website: Click here |
The International Solid-State Circuits Conference is the main global forum for presenting technological advancements in solid-state circuits and systems-on-chip, offering a unique opportunity for engineers working at the cutting edge of IC design and application to stay up to date on innovations, and to network with leading experts.
A member of the European Subcommittee, STMicroelectronics is jointly presenting two papers this year, in addition to chairing one of the sessions.
Join us for these sessions to know more!
Date | Time (PST) | Title | Speaker |
17 Feb | 7am | Session Moderator Innovations in Low-Power and Secure IoT | F. Gianesello – STMicroelectronics |
17 Feb | 8:46am | Paper presentation A 1.25GHz Fully Integrated DC-DC Converter Using Electromagnetically Coupled Class-D LC Oscillators | A. Novello1, G. Atzeni1, G. Cristiano1, M. Coustans2, T. Jang1 1 ETH Zurich, Zurich, Switzerland 2 STMicroelectronics, Switzerland |
17 Feb | 8:54am | Paper presentation A 250GHz Autodyne FMCW Radar in 55nm BiCMOS with Micrometer Range Resolution | S. H. Naghavi1, S. Seyedabbaszadehesfahlani1, F. Khoeini1, A. Cathelin2, E. Afshari1 1 University of Michigan, Ann Arbor 2 STMicroelectronics, France |