Footprint of a SiC Diode

Discover the environmental impact of a SiC Diode

Climate change

Total impact
124
Kg CO2-eq.
Or
1240
km by car
Assuming 100g/km
5 life cycle stages
Raw materials
ST production site
Transport
Use
End-of-life

Hover the section to discover the footprint of each life cycle stage

The contribution of the use phase to all impact categories is so high that all other life cycle phases can be neglected

Climate change

124
Kg CO2-eq.
Total impact
Or
1240
km by car
Assuming 100g/km
The raw materials have a negligible contribution to all indicators.

Silicon

54%

Direct materials (BE)

44%

Indirect materials

3%
The manufacturing has a negligible contribution to all indicators.

Energy consumption (including Renewable Energy)

75%

Air emissions

24%

Solid wastes

0%

Water consumption

1%

Water emissions

0%
The product transportation between ST sites has a negligible impact.
The use stage is virtually the sole contributor to all impact categories. The use case scenario chosen is representative of a use in data centre power supply.
The end-of-life has a negligible impact compared to other product life phases.

*This Life-Cycle-Assessment (LCA) results showcase the main footprint contributors for several ST product families. The results should be considered in isolation unless subsequent LCA conditions can be fully replicated. The results are based on the LCA methodology developed by ST and have not been subject to an external critical review process.

Sustainable growth needs

As the development of electronic goods continues to increase, it is imperative to understand the increasingly stringent environment, health and safety product requirements along with opportunities for sustainable production and consumption.ST commitment to eco-design is well established in EHS Decalogue. ST has identified Life Cycle Assessment (LCA) as the most appropriate methodology to calculate products carbon and water footprint and to highlight opportunities for ecological improvements in products design.

What is Life Cycle Assessment?

LCA is an internationally recognized approach that evaluates the potential environmental and human health impact associated with products and services throughout their life cycle, beginning with raw material extraction and including transportation, production, use, and end-of-life treatment. The LCA methodology is defined by ISO standards (ISO 14040, 2006; ISO 14044, 2006).

Objectives, goal and scope

ST has performed several complete LCAs for representative products, in line with ISO standards. Here is presented, as an example, the results pertaining to a product family. The LCA results presented here are limited to the objectives, goal and scope of this communication tool; therefore the aim is not to be comprehensive and only four selected environmental indicators are presented.