Footprint of an automotive MCU

Discover the environmental impact of an Automotive MCU (Stellar)

Climate change

Total impact
5720
g CO2-eq.
Or
57
km by car
Assuming 100g/km
5 life cycle stages
Raw materials
ST production site
Transport
Use
End-of-life

Hover the section to discover the footprint of each life cycle stage

The use phase is by far the largest contributor to all the considered impact categories.

Climate change

5720
g CO2-eq.
Total impact
Or
57
km by car
Assuming 100g/km
The main contribution within raw materials is Silicon wafer production.

Silicon

60%

Direct materials (BE)

26%

Indirect materials

14%
For all the indicators except water use, the manufacturing energy consumption is the main contributor to the ST production site impact.

Energy consumption (including Renewable Energy)

82%

Air emissions

16%

Solid wastes

0%

Water consumption

2%

Water emissions

0%
The product transportation between ST sites has a low impact.
The use stage has the highest contribution to all indicators. The use case scenario is representative a use in electric car for controling an on-board charger (OBC).
The end-of-life has a negligible impact compared to other product life phases.

*This Life-Cycle-Assessment (LCA) results showcase the main footprint contributors for several ST product families. The results should be considered in isolation unless subsequent LCA conditions can be fully replicated. The results are based on the LCA methodology developed by ST and have not been subject to an external critical review process.

Sustainable growth needs

As the development of electronic goods continues to increase, it is imperative to understand the increasingly stringent environment, health and safety product requirements along with opportunities for sustainable production and consumption.ST commitment to eco-design is well established in EHS Decalogue. ST has identified Life Cycle Assessment (LCA) as the most appropriate methodology to calculate products carbon and water footprint and to highlight opportunities for ecological improvements in products design.

What is Life Cycle Assessment?

LCA is an internationally recognized approach that evaluates the potential environmental and human health impact associated with products and services throughout their life cycle, beginning with raw material extraction and including transportation, production, use, and end-of-life treatment. The LCA methodology is defined by ISO standards (ISO 14040, 2006; ISO 14044, 2006).

Objectives, goal and scope

ST has performed several complete LCAs for representative products, in line with ISO standards. Here is presented, as an example, the results pertaining to a product family. The LCA results presented here are limited to the objectives, goal and scope of this communication tool; therefore the aim is not to be comprehensive and only four selected environmental indicators are presented.