Footprint of a MEMS

Discover the environmental impact of a MEMS

Climate change

Total impact
80
g CO2-eq.
Or
0.8
km by car
Assuming 100g/km
5 life cycle stages
Raw materials
ST production site
Transport
Use
End-of-life

Hover the section to discover the footprint of each life cycle stage

The raw materials and the ST production site are the major contributors to all the considered impact categories. Together, they represent nearly 80% of all the impacts.

Climate change

80
g CO2-eq.
Total impact
Or
0.8
km by car
Assuming 100g/km
The raw materials have a high contribution to all the indicators. It is the second contributing stage for all indicators mainly due to the use of silicon as raw material.

Silicon

88%

Direct materials (BE)

1%

Indirect materials

11%
The ST production site has the highest contribution to all the indicators. For all the indicators except water use, the manufacturing energy consumption is the main contributor to the ST production site impact.

Energy consumption (including Renewable Energy)

69%

Air emissions

29%

Solid wastes

0%

Water consumption

2%

Water emissions

0%
The transport between ST sites has a small impact.
The use stage has a contribution of around 20% for most indicators. However, the impact of the use stage is highly dependent on the type of application of the MEMS. The scenario for this calculation is representative of a chip in a wearable device such as a smart watch. The sensor with build-in AI can save more energy in the application than it consumes, thanks to a wake-up function.
The end-of-life has a negligible impact compared to other life cycle stages. However, this impact may vary according to how the end-of-life MEMS will be disposed.

*This Life-Cycle-Assessment (LCA) results showcase the main footprint contributors for several ST product families. The results should be considered in isolation unless subsequent LCA conditions can be fully replicated. The results are based on the LCA methodology developed by ST and have not been subject to an external critical review process.

Sustainable growth needs

As the development of electronic goods continues to increase, it is imperative to understand the increasingly stringent environment, health and safety product requirements along with opportunities for sustainable production and consumption.ST commitment to eco-design is well established in EHS Decalogue. ST has identified Life Cycle Assessment (LCA) as the most appropriate methodology to calculate products carbon and water footprint and to highlight opportunities for ecological improvements in products design.

What is Life Cycle Assessment?

LCA is an internationally recognized approach that evaluates the potential environmental and human health impact associated with products and services throughout their life cycle, beginning with raw material extraction and including transportation, production, use, and end-of-life treatment. The LCA methodology is defined by ISO standards (ISO 14040, 2006; ISO 14044, 2006).

Objectives, goal and scope

ST has performed several complete LCAs for representative products, in line with ISO standards. Here is presented, as an example, the results pertaining to a product family. The LCA results presented here are limited to the objectives, goal and scope of this communication tool; therefore the aim is not to be comprehensive and only four selected environmental indicators are presented.