Footprint of an Ultra Low Power MCU

Discover the environmental impact of an Advanced Power-saving Microcontroller

Climate change

Total impact
120
g CO2-eq.
Or
1.2
km by car
Assuming 100g/km
5 life cycle stages
Raw materials
ST production site
Transport
Use
End-of-life

Hover the section to discover the footprint of each life cycle stage

The use phase and the manufacturing are the major contributors to all the considered impact categories. Together, they represent above 90% of all the impacts.

Climate change

120
g CO2-eq.
Total impact
Or
1.2
km by car
Assuming 100g/km
The raw materials have a high contribution to all the indicators. It is the second contributing stage for most indicators mainly due to the use of silicon as raw material.

Silicon

88%

Direct materials (BE)

0%

Indirect materials

12%
The ST production site is highest contributor to all the indicators. For all the indicators except water use, the manufacturing energy consumption and air emissions are the main contributors to the ST production site impact.

Energy consumption (including Renewable Energy)

48%

Air emissions

47%

Solid wastes

0%

Water consumption

4%

Water emissions

0%
The product transportation between ST sites has a low impact.
The product is designed for low power consumption in use, thus the low environmental impact of this phase. The scenario taken is representative of a use in a smart watch.
The end-of-life has a negligible impact compared to user life cycle stages. This impact may vary according to how the product will be disposed of.

*This Life-Cycle-Assessment (LCA) results showcase the main footprint contributors for several ST product families. The results should be considered in isolation unless subsequent LCA conditions can be fully replicated. The results are based on the LCA methodology developed by ST and have not been subject to an external critical review process.

Sustainable growth needs

As the development of electronic goods continues to increase, it is imperative to understand the increasingly stringent environment, health and safety product requirements along with opportunities for sustainable production and consumption.ST commitment to eco-design is well established in EHS Decalogue. ST has identified Life Cycle Assessment (LCA) as the most appropriate methodology to calculate products carbon and water footprint and to highlight opportunities for ecological improvements in products design.

What is Life Cycle Assessment?

LCA is an internationally recognized approach that evaluates the potential environmental and human health impact associated with products and services throughout their life cycle, beginning with raw material extraction and including transportation, production, use, and end-of-life treatment. The LCA methodology is defined by ISO standards (ISO 14040, 2006; ISO 14044, 2006).

Objectives, goal and scope

ST has performed several complete LCAs for representative products, in line with ISO standards. Here is presented, as an example, the results pertaining to a product family. The LCA results presented here are limited to the objectives, goal and scope of this communication tool; therefore the aim is not to be comprehensive and only four selected environmental indicators are presented.