Industrial Smart buildings NanoEdge AI Studio Predictive maintenance Gyroscope

AI solution for industrial predictive maintenance with NKE Watteco

Predictive maintenance solution for industrial equipment.

AI solution for industrial predictive maintenance with NKE Watteco
Industrial Smart buildings NanoEdge AI Studio Predictive maintenance Gyroscope
NKE Watteco leveraged STMicroelectronics ecosystem to develop an Artificial Intelligence solution that adds predictive maintenance features to any industrial equipment. Predictive maintenance solutions reduce equipment downtime, increase productivity, and optimize human intervention. 
The Bob Assistant, based on STMicroelectronics technology, is now installed in dozens of industrial sites across Europe and provides 24/7 predictive maintenance for thousands of pieces of equipment, such as pumps, air conditioners, engines and HVACs.
Jean-Claude Le Bleis
President at NKE Watteco

Approach

This solution can be adapted to any industrial equipment. The on-device learning capability of the NanoEdge AI Libraries can perform incremental learning to tailor the model to a specific piece of equipment in every environment. The solution can then detect any change in real time and with a high level of accuracy. It can send alerts to inform the maintenance teams, so they can carry out physical adjustments before major failures occur. This is achieved thanks to the Machine Learning algorithm running on an ultra-low power STM32 microcontroller.

Sensor

Accelerator from STMicroelectronics.

Code optimized with

NanoEdge AI Studio

Code optimized with

Running on

STM32

Running on

Resources

Code optimized with NanoEdge AI Studio

A free AutoML software for adding AI to embedded projects, guiding users step by step to easily find the optimal AI model for their requirements.

Code optimized with NanoEdge AI Studio

Running on STM32

The STM32 family of 32-bit microcontrollers based on the Arm Cortex®-M processor is designed to offer new degrees of freedom to MCU users. It offers products combining very high performance, real-time capabilities, digital signal processing, low-power / low-voltage operation, and connectivity, while maintaining full integration and ease of development.

Running on STM32

You also might be interested by

Industrial | Transportation

Smart asset tracking

Packages condition classification on sensors.

Industrial | Smart offices

Low-power anomaly detection on a fan

Low-power anomaly detection solution running on a sensor.

Industrial | Smart offices | Smart buildings | Smart homes

Face identification with ID3 Technologies

End-to-end AI solution for face identification running on STM32 microcontrollers.