Industrial Transportation Smart offices Smart buildings Appliances STM32Cube.AI Predictive maintenance Microphone

Fan anomaly classification based on ultrasound analysis 

Neural Network classification based on a high-frequency analog microphone pipeline.

Fan anomaly classification based on ultrasound analysis 
Start with the Function Pack
Industrial Transportation Smart offices Smart buildings Appliances STM32Cube.AI Predictive maintenance Microphone
Start with the Function Pack
Machines interact with their environment by emitting various signals. These signals are source of relevant information reflecting equipment functioning. Being able to understand these signals allows significant optimization capabilities. For example, before an anomaly or failure occurs, your machine generates slightly abnormal vibration pattern, noise and ultrasounds. By placing a sensor on the machine, we can monitor its activity. Thanks to Artificial Intelligence, we can create smart solution which will distinguish abnormality. As a result, the equipment can automatically classify the criticality of an anomaly and send relevant alert to maintenance team. We have implemented this approach on a fan motor for demonstration purposes, but this approach can easily be adapted to many industrial machines.

Approach

In this use case, we used the FP-AI-MONITOR1 function pack to simplify the application development. It is a complete integration of an artificial neural network coupled with pre/post-processing functions and connected to microcontroller peripherals.

The ultrasound-based classification model takes almost one second of data, then preprocesses it using the mel-frequency cepstral coefficients (MFCC), and then feeds it to a pre-trained neural network. The network is trained for four classes [ 'Off', 'Normal', 'Clogging', 'Friction' ].The ultrasound-based classification captures audio at a 192 kHz (16-bit, 1 channel) rate using the on-board analog MEMS microphone. Every millisecond, a DMA interrupt is received with the last 192 audio samples. These samples are then accumulated in a sliding window consisting of 4096 samples with no overlap. The buffer is injected every 21,33 ms into USC preprocessing for feature extraction. The USC preprocessing extracts ultra sound features: MFCC (46x32) spectrogram.

For computational efficiency and memory management optimization, the step is divided into two routines: 
- The first part computes one of the 46 MFCC columns from the time domain input signal into the Mel scale using FFT and Filter bank applications (32 mel bands). 
- The second part, when all 32 columns have been calculated (i.e., after 981 ms), a log scaling is applied to the mel scaled spectrogram, creating the input feature for the USC convolutional neural network. 

Every 981 ms, the (46x32) MFCC spectrogram is fed to the USC convolutional neural network input. The Model classifies anomalies among four classes: [ 'Off', 'Normal', 'Clogging', 'Friction']. This model is created to work for a USB fan when the fan is running at the maximum speed and does not work very well when tested on other speeds 

Sensor

Analog MEMS microphone with frequency response up to 80 kHz (reference: IMP23ABSU)

Data

Data format 2-3 hours data recorded in various condition, balanced among the four classes at a fixed speed of 1500 rpm. 

Results

Model ST Convolutional Neural Network Quantized
Input size: 46x32
Complexity: 565 K MACC
Memory footprint:
163 KB Flash for weights 
74 KBRAM for activations 
Performance on STM32L4R9 (Low Power) @ 120 MHz
Pre-processing: 24 MHz; 46 MFCC column computation per second, 4,2 ms per column
NN processing: 1 inference per second; 10 MHz, 78 ms per inference
Confusion matrix 

Optimized with

STM32Cube.AI

Optimized with

Compatible with

STM32L4 series

Compatible with

Resources

Optimized with STM32Cube.AI

A free STM32Cube expansion package, X-CUBE-AI allows developers to convert pretrained AI algorithms automatically, such as neural network and machine learning models, into optimized C code for STM32.

Optimized with STM32Cube.AI

Compatible with STM32L4 series

The STM32 family of 32-bit microcontrollers based on the Arm Cortex®-M processor is designed to offer new degrees of freedom to MCU users. It offers products combining very high performance, real-time capabilities, digital signal processing, low-power / low-voltage operation, and connectivity, while maintaining full integration and ease of development.

Compatible with STM32L4 series

You also might be interested by

Transportation

Enhanced safety and lifetime of e-assisted bikes with Panasonic

Tire pressure monitoring solution to improve rider safety and convenience.

Industrial | Transportation

Smart asset tracking

Packages condition classification on sensors.

Industrial | Smart offices

Low-power anomaly detection on a fan

Low-power anomaly detection solution running on a sensor.