Classification of the net vibrations with an accelerometer.
Did the ball hit the net? For all the ping pong games with no official referee, we developed a smart sensor that can detect when the ball hits the table or the net using machine learning! This application is easily transferable to other use cases using NanoEdge AI Studio.
2 classes (let & normal play):
100 % accuracy, 0.8 KB RAM, 0.2 KB Flash
3 classes:
95 % accuracy, 0.8 KB RAM, 0.5 KB Flash
A green point means we are able to correctly predict if the finish will pass a visual inspection or not.
A red point means we were incorrect.
A free AutoML software for adding AI to embedded projects, guiding users step by step to easily find the optimal AI model for their requirements.
The STM32 family of 32-bit microcontrollers based on the Arm Cortex®-M processor is designed to offer new degrees of freedom to MCU users. It offers products combining very high performance, real-time capabilities, digital signal processing, low-power / low-voltage operation, and connectivity, while maintaining full integration and ease of development.