An innovative approach to measure people flows using an in-house thermal sensor.
Making buildings smarter to improve their efficiency is one of the biggest challenges companies have to face. The people flow counting sensor developed by Schneider Electric in partnership with STMicroelectronics enables the counting of the number of people. It also detects whether they are crossing a virtual line in both directions, using a large field of view and a small resolution thermal sensor.
“
This promising technology opens a new solution for attendance monitoring and people counting in numerous applications such as monitoring queues, building usage, and social distancing. Our innovative demonstration, created with STMicroelectronics, finds applications in various segments, from hotels to offices and retail, and more generally any building where knowing attendance and space occupation has a value. This will redefine the building of the future!”
Maxime Loidreau, IoT Sensors Program Manager at Schneider Electric
A free STM32Cube expansion package, X-CUBE-AI allows developers to convert pretrained AI algorithms automatically, such as neural network and machine learning models, into optimized C code for STM32.
The STM32 family of 32-bit microcontrollers based on the Arm Cortex®-M processor is designed to offer new degrees of freedom to MCU users. It offers products combining very high performance, real-time capabilities, digital signal processing, low-power / low-voltage operation, and connectivity, while maintaining full integration and ease of development.