Predictive maintenance is a maintenance strategy that uses machine learning to predict when equipment is likely to fail.
Industrial equipment, such as water pumps, produce different signals during operation. By placing sensors on these pieces of equipment for data collection, it is possible to use machine learning to recognize normal and abnormal behavioral patterns. This proactive approach aims at minimizing downtime, increasing efficiency, and extending equipment lifespan.
We implemented the following approach on a water pump: we collected and analyzed its vibrations and used a machine learning model to detect anomalies. This approach can easily be adapted to many other industrial machines. 

Approach

Project goals:
  • detect anomalies in a hydraulic circuit equipped with a pump by using the vibrations of the pump.
  • show that our model can be used on a completely different integrated circuit and is still able to detect anomaly thanks to our edge AI learning technology.

In this project, we used a first circuit to log the vibration data of the pump using an accelerometer. We gathered both normal and abnormal signals, which were created by closing the taps that diverted the flow of water.
We then created an anomaly detection model in the NanoEdge AI Studio. The software tool generated the most optimized model for our learning data.
The model created was loaded on a STEVAL-PROTEUS1 and connected to a first circuit. This prototype allowed us to detect both normal and abnormal data in real time.
We then moved the Proteus board containing the model to a second circuit. We used on-edge learning to retrain the same model with the signals of the new circuit in few seconds. The model performed well on the new circuit, even if it was originally optimized for the first one.

Sensor

Accelerometer (3-axis): ISM330DHCX

Data

Regular and abnormal signals
- Regular signals: 640 signals of pump vibrations with the first circuit in a normal state
- Abnormal signals: 440 signals of pump vibrations with one of both deviations blocked
Signal length 768 (256 per axis, 3 axes)
Data rate 6667 Hz, range: 2g

Results

Anomaly detection classes:
100% accuracy, 7.8 Kbytes RAM, 6.1 Kbytes Flash

uc-neais-results-pump-anomaly_detection-based-on-vibrations uc-neais-results-pump-anomaly_detection-based-on-vibrations uc-neais-results-pump-anomaly_detection-based-on-vibrations

Blue points represent the normal signals, red points the abnormal ones. 
The signal values are on the abscissa axis and the confidence level of the prediction is shown on the ordinate

Model created with
NanoEdge AI Studio
NanoEdge AI Studio
Compatible with
STM32 series
STM32 series

Resources

Model created with NanoEdge AI Studio

A free AutoML software for adding AI to embedded projects, guiding users step by step to easily find the optimal AI model for their requirements.

NanoEdge AI Studio NanoEdge AI Studio NanoEdge AI Studio

Compatible with STM32 series

The STM32 family of 32-bit microcontrollers based on the Arm Cortex®-M processor is designed to offer new degrees of freedom to MCU users. It offers products combining very high performance, real-time capabilities, digital signal processing, low-power / low-voltage operation, and connectivity, while maintaining full integration and ease of development.

STM32 series STM32 series STM32 series

You might also be interested by

Entertainment | Image recognition | Vision | STM32Cube.AI | Demo | Tutorial | GitHub | Video

Smart mirrors for fitness: pose estimation and multi-person tracking

Track and analyze users' body movements to provide feedback on exercise with STM32N6 at 28 FPS.

Predictive maintenance | Accelerometer | NanoEdge AI Studio | Video | Partner | Industrial

Anomaly detection with on-device learning with Rtone

Anomaly detection solution on industrial equipment, running on STM32 MCU.

Object detection | Vision | STM32Cube.AI | Idea | GitHub | Video | Dataset | Smart building

Personal protective equipment detection

Detection of personal protective equipment on workers using an object detection AI model.