Interactive Block Diagram
Block Diagram
HDBaseT for in-vehicle connectivity
The HDBaseT Automotive technology is the solution to the in-vehicle connectivity challenges. It is a derivative of HDBaseT, a mature, proven and standardized technology for the transmission of high-definition audio and video, controls, Ethernet, USB and even power in the consumer electronics and professional audiovisual markets. This combination of high bandwidth, high performance, feature-rich capabilities, and an existing infrastructure makes an HDBaseT solution ideal for in-vehicle networking.
STMicroelectronics and Valens
STMicroelectronics and Valens have worked closely to enable HDBaseT Automotive technology to be built into the next-generation of connected cars. The highly efficient technology optimizes in-vehicle connectivity by enabling the transmission of reliable 6 Gbps high-throughput infotainment, road safety, and automotive-control content over a low-cost infrastructure with near-zero latency. Valens, as the inventor of HDBaseT and founder of the HDBaseT Alliance, brings the technology and expertise to accomplish the goal of commercializing HDBaseT-enabled vehicles; STMicroelectronics contributes with its extensive design and manufacturing experience and in-depth knowledge of compliance with the strict automotive quality and reliability requirements. Further information about Valens can be found at: www.valens.com