Save to myST

Mobile base station

A mobile base station, also called a base transceiver station (BTS), is a fixed radio transceiver in any mobile communication network or wide area network (WAN). The base station connects mobile devices to the network and routes them to other terminals in the network or to the core network of a mobile operator.
The network can be based on any of the wireless communication technologies like GSM, CDMA, 3G, 4G, 5G, and 6G mobile networks, WiMAX broadband, as well as wi-fi connectivity. A typical base transceiver station consists of multiple subsystems, including:
  • The baseband unit (BBU), processing all baseband signals and connecting the base station to the core network of the mobile operator via optical fiber.
  • The radio unit or remote radio unit (RRU), amplifying and transmitting the radio signals received from the BBUs to the antenna.
  • The active antenna system (AAS) introduced in the recent mobile networks (5G and beyond) to support multiple transmit and multiple receive techniques (mMIMO) based on antenna arrays.
Read more

Active Antenna System (AAS)

An active antenna system (AAS) in a mobile base station is a transceiver that integrates an antenna and radio frequency (RF) components in a single unit. This integration improves performance in mobile networks and enables some of the following advan
View application

Baseband Unit (BBU)

The baseband unit (BBU) is a crucial component in mobile base stations, handling tasks like signal processing, resource allocation, and protocol management to ensure efficient communication between mobile devices and networks. It also ensures securit
View application

Remote Radio Unit (RRU)

A remote radio unit (RRU), commonly referred to as a Remote Radio Head (RRH), is a transceiver that you'll find on wireless base stations. These transceivers connect wireless devices with wireless networks. RRUs have become one of the most important
View application

Key challenges

Mobile base station designers often need to manage the following aspects:

  • Compatibility for integrating base transceiver stations between different vendors' equipment.
  • Scalability in ensuring that the base station can scale to support multiple and new protocols to meet the growing demand for mobile services.
  • Energy efficiency to reduce the mobile base station carbon footprint.
  • Security, authentication, privacy, and regulatory compliance to ensure that mobile networks are secure and reliable.

Our products and solutions

ST answers these challenges by providing a wide range of innovative products to the market.
Our offering includes an extensive range of 32-bit microcontrollers and microprocessors equipped with a set of hardware peripherals and software development tools.

Secure ST solutions include a product family as part of a complete ecosystem to support authentication, secure connection establishment, secure boot and firmware upgrade, and trusted network access.

ST provides a complete power device portfolio, including IGBTs, thyristors, power rectifiers and MOSFETs, power modules and system-in-package (SiP) solutions to make mobile base stations more energy-efficient.

Our broad range of inertial and environmental MEMS sensors can also enhance the functionality of base transceiver stations.