Amazon Sidewalk is a groundbreaking shared network designed to enhance the connectivity and functionality of compatible devices. By leveraging Sidewalk relays (Bridges), such as select Echo and Ring devices, it extends the coverage of low-bandwidth networks, ensuring that devices remain connected to the cloud even beyond the confines of home perimeter.
This innovative and standardized technology opens the door to a host of new experiences, including seamless item location and enhanced control of smart home services.
Amazon Sidewalk is built with robust privacy and security measures to safeguard customer data, providing peace of mind while enjoying the benefits of a more connected environment.
Applications
- In an Amazon Sidewalk network, connected devices play crucial roles in ensuring seamless connectivity and expanded functionalities. Here are the key roles of connected devices within the Amazon Sidewalk network:
- Sidewalk Bridge Devices (relays): These devices, like Echo and Ring devices, connect sidewalk enabled devices to the Sidewalk network and to the internet. They extend the network's coverage, enabling compatible devices to remain connected even when outside the range of traditional home Wi-Fi networks.
- Sidewalk-enabled Devices: These end-user devices connect to the Sidewalk network using the network created by the Sidewalk Bridges. Variety of application apply to this Sidewalk-enabled devices like smart lights, pet trackers, and sensors. This connectivity enhancement significantly augments the overall functionality of these devices.
- Wide Area Community Networking: Contributing to the Network: When within range of a Sidewalk Bridge device, connected devices contribute a fraction of their internet bandwidth to the Sidewalk network. This collective contribution fosters a shared network, ensuring continuous connectivity and vital updates for all connected devices, even in the absence of traditional Wi-Fi networks.
- Key features of Amazon Sidewalk:
- Low bandwidth: small amounts of data are transmitted, allowing extended battery lifetime for end devices usually battery powered.
- Extended range: thanks to wireless technology and community networking capability, devices stay connected over longer distances than local Wi-Fi allows.
Sidewalk Coverage Maps - Security: encryptions are used to protect data shared across the network.
- Technologies used to build Amazon Sidewalk:
- Bluetooth LE used for short range between devices with low power consumption profile and for easy initial device set up. Connectivity is up to few hundred meters, or beyond front-door range.
- Sub-1GHz FSK (Frequency Shift Keying modulation) used for data transmission between devices and to the Bridges, up to a long-range of about 1Km, or beyond the fence range (referred as synchronous HDR: High Distance Range)
- Sub-1GHz CSS (Chirp-Spread-Spectrum modulation) used for long distance communication between devices extending the reach of connected devices (up to about 10 kilometers), or sub-urban range (referred as asynchronous LDR: Long Distance Range)
The protocol makes currently use of three optional wireless technologies, enabling incrementally extend connectivity area coverage from short-range to urban or rural areas.
- Sidewalk-enabled devices can be built based on:
- Bluetooth® LE only
- Bluetooth® LE + Long-range (FSK)
- Bluetooth® LE + Long-range (FSK & LoRa)
Understanding these roles and required technologies is pivotal when selecting microcontrollers with embedded wireless features, as it underscores the importance of seamless connectivity and network contribution within the Amazon Sidewalk ecosystem.
Product types
STM32WBA5 and STM32WL5 wireless MCUs series are suitable and fully supporting any kind of Amazon sidewalk device type.
The STM32WBA is based on an Arm® Cortex® M33 running at 100MHz with TrustZone ® technology; it supports Bluetooth® Low Energy 5.4 with security assets required to ensure Amazon Sidewalk security criteria
The STM32WL5 is fully compatible with Amazon Sidewalk supporting the LoRa and FSK modulations. It is based on a dual core, Arm® Cortex® M4 & M0+ running at 48 MHz.
The STM32WBA5 combined with the STM32WL5 solution is an Amazon Sidewalk qualified solution and provides a future-proof scalability of the application, both in terms of processing capabilities and memory footprints. Moreover, the dual-chip partitioning allows to create innovative and flexible coding architecture safeguarding the device security features during lifetime operations, such as firmware upgrade (FUOTA).
For more streamlined application requirements it’s also possible to replace the STM32WL5 wireless MCU with a more cost-effective S2-LP Sub-GHz FSK transceiver, besides the STM32WBA5. This solution will provide BLE + FSK enabled coverage (no CSS modulation supported) capable of addressing a wide variety of connectivity range requirements.
The STM32WBA55 and STM32WL5 MCUs are available on the NUCLEO-WBA55CG and NUCLEO-WL55JC1. The S2-LP is available as an expansion kit with the X-NUCLEO-S2915A1
Other Sidewalk benefits
Amazon Sidewalk is designed to provide a secure, easy-to-use, and efficient way to extend the connectivity and utility of smart devices. As with any technology, users should consider their own needs and privacy preferences when deciding to participate in the network.
- Improved reliability:
- Redundancy: Devices can connect to a nearby Sidewalk Bridge if their connection fails, ensuring they stay online.
- Stability: Sidewalk provides consistent connections, even for devices in areas with poor connectivity.
- Simplified setup and use:
- Ease of setup: Devices connect to Sidewalk automatically, requiring minimal user effort.
- User-friendly: Amazon manages the network's complexity, making it seamless for users.
- Community support:
- Neighborhood network: Helps locate pets or valuables with compatible tracking devices.
- Collective benefits: The network grows stronger and more supportive as more users join.
- Device compatibility:
- Broad ecosystem: Compatible with various devices like lights, sensors, and trackers for a versatile smart device ecosystem.
- Cost-efficiency:
- No additional fees: Utilizes a small portion of your home's Wi-Fi bandwidth without extra charges.
- Resource sharing: Efficient operation by sharing internet bandwidth, eliminating the need for separate data plans.
- Innovation and development:
- Developer support: Amazon invites developers to create new applications and devices for the Sidewalk network.
- Future possibilities: The network is poised to support an expanding range of IoT devices and services.
- Always upgradable fleet:
- Automatic Updates: Devices receive firmware updates automatically for continuous improvements in functionality and security.