Different types of coffee beans have distinct flavors that can be enhanced or diminished during the roasting process. By recognizing the type of bean being used, a coffee machine can adjust its brewing parameters to bring out the best flavor in each type of bean.

Approach

The use case presented is based on a coffee bean dataset to recognize the level of roasting. The solution proposes a model trained on a public dataset providing very good accuracy while running on an STM32.
This model was trained thanks to the Python scripts provided in the STM32 model zoo (read our tutorial on the training to learn more).
Here, after setting up our STM32 Model Zoo project, we downloaded the dataset and placed it in the appropriate structure.
Then we updated the yaml file, which was used to configure the training, with the following settings:
general:
project_name: coffee_bean
dataset:
name: coffee
class_names: [Green, Light, Medium, Dark]
training_path: datasets/train
validation_path:
test_path: datasets/test
Feel free to adjust those settings according to your use-case.
Finally, we simply ran the "train.py" script.

train.py_python_script train.py_python_script train.py_python_script

You will find everything you need in the STM32 model zoo to train and retrain the model with your own data. The model can also be easily deployed on a STM32H747 discovery kit with the Python scripts provided in the repository (read our tutorial on the deployment to learn more).
You can find details of all these steps in our Getting started video.

Sensor

Vision: Camera module bundle (reference: B-CAMS-OMV)

Data

Dataset Coffee Bean Dataset Resized (224 X 224) (License CC BY-SA 4.0)
Data format:
There are four roasting levels. The green or unroasted coffee beans, a lightly roasted coffee bean, a medium-roasted and dark roasted. The camera is set at a location with a plane parallel to the objects path when photographs are being captured. There are 4800 photos in total, classified in 4 degrees of roasting and resized to a resolution of 224x244. There are 1200 photos under each degree.

Results

Model MobileNetV2 alpha 0.35
Input size: 128x128x3
Memory footprint of the quantized model:
Total RAM: 260 KB

  • RAM activations: 224 KB
  • RAM runtime: 36 KB


Total Flash: 528 KB

  • Flash weights: 406 KB
  • Estimated flash code: 122 KB


Accuracy:
Float model: 97.75%
Quantized model: 97.25%
Performance on STM32H747 (High-perf) @ 400 MHz 
Inference time: 107 ms
Frame rate:  9.3 fps

use-case-stm32-cube-ai-confusion-matrix-coffee-bean-recognition use-case-stm32-cube-ai-confusion-matrix-coffee-bean-recognition use-case-stm32-cube-ai-confusion-matrix-coffee-bean-recognition

Confusion matrix of the quantized model

Resources 

Model repository ST Edge AI Model Zoo

A collection of reference AI models optimized to run on ST devices with associated deployment scripts. The model zoo is a valuable resource to add edge AI capabilities to embedded applications.

ST Edge AI Model Zoo ST Edge AI Model Zoo ST Edge AI Model Zoo

Optimized with STM32Cube.AI

A free STM32Cube expansion package, X-CUBE-AI allows developers to convert pretrained AI algorithms automatically, such as neural network and machine learning models, into optimized C code for STM32.

STM32Cube.AI STM32Cube.AI STM32Cube.AI

Compatible with STM32H7 series

The STM32 family of 32-bit microcontrollers based on the Arm Cortex®-M processor is designed to offer new degrees of freedom to MCU users. It offers products combining very high performance, real-time capabilities, digital signal processing, low-power / low-voltage operation, and connectivity, while maintaining full integration and ease of development.

STM32H7 series STM32H7 series STM32H7 series
You might also be interested by

Tutorial | Demo | MEMS MLC | Gyroscope | Accelerometer | Predictive maintenance | Wearables

Recognize head gestures in wearable devices with ultra low power sensors

Recognize head gestures such as nodding, shaking, and other general head movements through the Machine Learning Core available in MEMS sensors.

Tutorial | Demo | MEMS MLC | Accelerometer | Industrial | Predictive maintenance

How to monitor and classify fan-coil systems with STWIN.box

Monitor and classify the behavior of a fan (e.g. on HVAC units) through the Machine Learning Core available in MEMS sensors.

Partner | Smart city | Transportation | Vision | STM32Cube.AI | STM32 AI MCU | Video

Number-Plate Recognition (ANPR) based on Vision AI by Irida Labs

Vision AI-powered solution for Automatic Number-Plate Recognition (ANPR) for smart city applications, running on STM32 MCUs