X-CUBE-IAP-SD

Active
Design Win

In-application programming with SD cards software expansion for STM32Cube (AN4854)

Get Software Get Software Download databrief

Product overview

Description

An important requirement for most Flash memory-based systems is the ability to update the firmware installed in the end product. This ability is referred to as in-application programming (IAP).

The X-CUBE-IAP-SD firmware package contains the source code of IAP examples based on STM32Cube.

For more details refer to the application note AN4854 available from www.st.com.

  • All features

    • Flash memory erase
    • Flash memory programming
    • SDCARD communication through SPI or SDMMC
    • Flash memory write protection configuration
    • Separation of application from loader

Get Software

A free-form description of a component.Software VersionProduct supplier(s)ECCNs are five character alpha-numeric designations used on the Commerce Control List to identify dual-use items for export control purposes.ECCNs are five character alpha-numeric designations used on the Commerce Control List to identify dual-use items for export control purposes.