ST @ The Things Conference Embedded 2022
ST @ The Things Conference Embedded | |
STM32 solutions are at the heart of Generic Node designs:
|
ST on stage | ||||
| ||||
| ||||
ST Speakers | ||||
Anicet Giaimo, Product Line Marketing Manager for wireless microcontrollers, STMicroelectronics Anicet is a Product Line Marketing Manager at STMicroelectronics. He began his career with ST in 2007 in Taiwan as a Field Application Engineer responsible for customer support for touch sensing and motor control MCU applications. In 2013, he started working as a Technical Marketing Engineer focused on the digital power MCU market. Since 2015 he has been working in France in ST’s Microcontroller Division as a Product Line Marketing Manager. He is responsible for the business development of ST’s ultra-low-power MCUs and is now in charge of the STM32WL, ST’s Sub-GHz wireless MCU. | ||||
Alec Bath, Applications Manager for wireless microcontrollers, STMicroelectronics Alec Bath is Applications Manager for wireless microcontroller products in the Americas. During his 21-year tenure at ST, Alec has supported a variety of 8-bit and 32-bit microcontroller architectures: 8051, ARM7, ARM9, and of course the highly successful ARM Cortex M-based STM32 families. Prior to ST, Alec worked as a hardware design engineer at Motorola for analog cellphones and automotive body electronics modules. His interests include competitive ultramarathoning, cycling, hiking, photography, woodworking, and electronics projects. |