20 Feb 2008 | Geneva

New-Technology Power MOSFET Family from STMicroelectronics Enables Higher Frequencies and Lower Losses in DC-DC Supplies

Extremely low ‘Figure of Merit’ MOSFETs in DPAK packages deliver lower conduction and switching losses: Up to 3W less in a typical voltage regulator module Geneva / 20 Feb 2008

In addition to the high efficiency, the new MOSFETs allow practical circuits to operate at higher-than-normal switching frequencies, enabling a reduction in the size of the circuit’s passive components. For example, a 10% increase in switching frequency can lead to a 10% reduction in passive components required by the output filter.

The STD60N3LH5 and STD85N3LH5 are the first in a new series of STripFET V devices which provide superior performance and increased efficiency as a result of low ON-resistance and significantly lower total gate charge. Both are 30V (BVDSS) devices. With gate charge (Qg) of just 8.8nC (nanocoulombs), and Rds(on) of 7.2 milliohms at 10V, the STD60N3LH5 is an ideal choice as a control FET in non-isolated DC-DC step-down converters. The 4.2 milliohm Rds(on) at 10V of the STD85N3LH5, with a Qg of 14nC, makes it an optimal choice as a synchronous FET. Both devices are produced in DPAK and IPAK packages and will be soon available in other package options including SO-8, PowerFLAT 3.3x3.3, PowerFLAT 6x5, and PolarPAK®. The new series of STripFET V devices are ideal for notebook, server, telecom and networking applications.

ST’s STripFET technology makes use of very high ‘equivalent cell density’ and smaller cell features to achieve extremely low ON-resistance and losses, while using less silicon area. STripFET V is the latest generation of this technology, achieving approximately 35% improvement in the critical indicator of silicon resistance and active area, plus some 25% reduction in total gate charge per active area, compared to the earlier generation.

Both devices are in full production. The STD60N3LH5 is priced at $0.65 in quantities of 2500 pieces, while the STD85N3LH5 is priced at $0.95 in quantities of 2500 pieces.

Further information is available at www.st.com/pmos

 Click here for the high-resolution photo

STripFET™ is a trademark of STMicroelectronics. PolarPAK is a registered trademark of Vishay Siliconix.


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2007, the Company's net revenues were $10.0 billion. Further information on ST can be found at www.st.com.
Information last updated Jan 2008