VL53L1X: A new generation, long distance ranging Time-of-Flight sensor based on ST’s FlightSense™ technology

Precision Ranging at the Speed of Light

Experience the cutting-edge performance of the newest Time-of-Flight long distance ranging sensor based on ST’s FlightSense™ technology

During this one-hour webinar, we will explore the benefits of the most advanced Time-of-Flight (ToF) sensor from the ST FlightSense™ product family, the VL53L1X. This innovative miniature ToF sensor is able to measure accurate distance up to 4 meters, and features a low-power autonomous mode for advanced user or object detection and ranging. Unlike conventional IR sensors, the VL53L1X uses ST’s latest generation ToF technology which allows absolute distance measurement regardless of the target color and reflectance.

Join us Wednesday, March 21st at 12 noon Central Time

You will learn:

  • The principles and advantages of ToF technology
  • The advanced integrated features of the VL53L1X sensor
  • The wide range of applications enabled by the VL53L1X

There will be a Q&A session at the end of the webinar to answer your questions real time.

There is no charge to participate in this event, but you must register through my.st.com.
 
If you have a myST accountRegister Now
If you do not have a myST accountCreate An Account


Not sure if you can make it? No problem! Register now and we will be sure to email you the recorded webinar.

詳細情報

The VL53L1X features highly-accurate ranging up to 4 meters and fast ranging frequency up to 50 Hz, all housed in a tiny reflowable package. The device integrates a SPAD receiving array, a 940 nm invisible Class1 laser emitter, physical infrared filters, and optics to achieve optimum ranging performance under various ambient lighting conditions over a wide range of cover-window options.