SecEdge was created by silicon industry veterans to address the unique security challenges of the growing edge Computing space. SecEdge provides a groundbreaking digital security platform for securing industrial controls, IoT, edge AI and edge Servers.
SecEdge platform is a comprehensive security and trust solution including:
- Strong Device security foundation
- Authentication – establishing or leveraging hardware root of trust and extending it into the application runtime, across various STMicroelectronics product families
- Trust Provisioning – Firmware TPM enabling crypto-agility and late binding of credentials for added supply chain security
- AI Model Protection and Management
- AI Model protection at rest and secure AI model update management
- Groundbreaking secure connectivity
- Patented technology to implement multiple IPSec tunnels from chip to cloud
- Ensure data privacy by separating data and management channels
- Prevent devices from being visible on the public Internet
- Patented technology to implement multiple IPSec tunnels from chip to cloud
- Development Agility
- Rapid integration and deployment tools to reduce time to market for secure products
Key advantages
- Single vendor, full-stack solution leaves no security gaps from edge to cloud
- Consistent security approach across STM32 MPU platforms reduces initial implementation and management costs
- Enables achieving compliance with new regulations such as CRA and NIST 800 guidelines
Products or services of SecEdge
SecEdge’s Digital Security Platform enables STM32MPU customers to rapidly deploy advanced secure connectivity from chip to cloud. It enables compliance with various regulations and recommendations across various industries and countries. The platform comprises several components:
Device Security
- SEC-TPM: is a TCG 2.0 compliant firmware TPM (fTPM) coupled with a TPM provisioning and attestation service that provides authentication and boot measurements for edge and IoT devices
- EmSPARK™ IoT Security suite: is a comprehensive device and application security software that makes use of hardware security capabilities provided by the STM32MPUs and extends it into the application runtime
Secure Connectivity
- MicroEdge™: is a Linux application deployed on the STM32MPUs that initiates multiple IPSec tunnels from STM32 devices. This establishes secure tunnels from device to cloud backends. MicroEdge™ can make use of STMicroelectronics' security ICs or other roots of trust such as TEEs.
SecEdge in STMicroelectronics ecosystem
SecEdge’s Secure connectivity solution extends the use of STM32 security features enabling a unique secure connectivity and device onboarding solution.
- Supports multiple STM32 root of trust options
- Secure Element ICs such as TPMs
- Arm TEEs
- Secure flash
- Device Provisioning
- Uses unique ID bound to Root of Trust (where available)
- Generates credentials and configures the device
- Network Isolation
- Reduces visible attack surface; isolates public internet interfaces to its own private network namespace
- Manages network stack features
- IPsec management
- Creates IPsec tunnels to cloud/data center end points
- Simplifies management; maps ports across NAT firewalls

製品・サービス:
• 組込み用ソフトウェア
• ソフトウェア開発ツール
所在地:
PO Box 201, 98024, Fall City, Washington, United States
お問合せ先:
Contact
ウェブサイト:
www.secedge.com
パートナー製品 | 概要 | 関連製品 | |
---|---|---|---|
MicroEdge™ | TURNKEY SECURITY AGENT FOR IOT DEVICES. MicroEdge® is an Edge security solution that enables the deployment of IPsec tunnels facilitating secure communications with other Cloud endpoint instances. | STM32MP1 series | |
EmSPARK™ IoT Security suite | Embedded security software and tools for ARM TrustZone enabled MPUs enabling secure boot and update, IP protection, lifecycle management | STM32MP1 series |
パートナー製品 | 概要 | 関連製品 | |
---|---|---|---|
SecEdge EmSPARK™ Security Suite SDK | SDK for integration of customer-developed TEE-resident Trusted Applications | STM32MP1 series |
免責条項
本ウェブサイトで定める利用規約、ST販売取引条件およびプライバシー・ポリシーに加えて、次の条件がすべてのSTMicroelectronicsのパートナー・プログラムに適用されます。
STMicroelectronicsはウェブサイト上で正確な情報を提供することに務めています。しかし、STMicroelectronicsは、情報の正確性ついて一切の責任を負いません。本ウェブサイト上でSTMicroelectronicsが提供するすべての情報は、あらゆる欠陥を含んだ「現状有姿」のままで提供され、明示、黙示または法定のものかを問わずいかなる種類の保証もありません。STMicroelectronicsは、そのパートナー・プログラム、製品またはサービスを、予告なく、いつでも変更または停止することができます。STMicroelectronicsのものではない製品またはサービスに関する言及は専ら情報提供のためのもので、STMicroelectronicsによる推奨を意味するものではありません。本ウェブサイトにおける「パートナー」という言葉または用語の使用は、STMicroelectronics と他の企業との間にパートナーシップ関係、代理関係、法的関係もしくは信認関係が存在すること、あるいは当該企業が何らかの意味においてSTMicroelectronicsの関連会社であることを示すものではなく、またこれを示唆するものでもありません。STMicroelectronicsのパートナー・プログラムにおけるパートナーは、その製品および/またはサービスならびに関連技術をSTMicroelectronicsの製品と共に購入または使用することについて個別のライセンスを提供致します。ライセンス条件、価格、サポート、当該パートナーの製品および/またはサービスに関するその他の情報については、該当するパートナーに直接お問い合わせください。当該製品および/またはサービスに係る取引条件はパートナー毎に異なる場合があり、また当該パートナーから直接かつ個別にライセンスされます。STMicroelectronicsは、パートナーが提案または提供する製品およびサービスの適切性についていかなる表明も保証も致しません。STMicroelectronicsは、パートナーが提供する製品またはサービスについて、明示、黙示または法定のものを問わず、あらゆる保証および条件(商品性、特定目的の適合性、権原、非侵害の保証および条件、または取引、使用もしくは取引慣行から生ずる保証および条件を含みますがこれらに限りません)をここに否認致します。 STMicroelectronicsは、直接損害、間接損害、付随的損害、特別損害、懲罰的損害、結果損害またはその他のあらゆる損害について、たとえ当該損害の可能性について告知を受けていたとしても、如何なる場合も責任を負いません。かかる損害は原因の如何を問わないものであり、また契約、厳格責任、不法行為(過失またはそれ以外を含む)を問わずいかなる責任理論に基づくかを問わないものであり、またパートナー・プログラムへのお客様の参加・信頼、パートナーの製品および/またはサービスのお客様による使用、若しくはお客様がこれらを使用、購入できないこと、またはかかる製品およびサービスの性能、お客様とパートナーとの関係、STMicroelectronicsポータルまたは当該ポータルにおいてSTMicroelectronicsから提供される情報をお客様が使用すること、または使用できないこと、あるいは当該情報に対する信頼から生ずる、またはこれらに関連して生ずる使用、利益または収入の喪失を含みますが、これらに限るものでなく、損害発生の種類を問いません。STMicroelectronicsが提供するサードパーティーのウェブサイトへのリンクは、STMicroelectronicsの管理下になく、STMicroelectronicsは、リンク先のサイトまたはリンク先のサイトに含まれるリンクに在るコンテンツ、資料、意見、助言もしくは声明、また当該コンテンツおよび資料の正確性または信頼性、また当該サイトの変更もしくは更新について一切責任を負いません。STMicroelectronicsは、リンク先のサイトで受信するいかなる形式の通信(ウェブ放送または音声通信を含むがこれらに限らない)についても責任を負いません。リンク先のサイト、リン先のサイトに含まれるリンクへのアクセスはお客様ご自身のリスクで行ってください。STMicroelectronicsは、専ら便宜のためにお客様にこれらのリンクを提供しているものであり、リンクが含まれていても、STMicroelectronicsによるサードパーティーのウェブサイトの保証(明示、黙示、その他を問わない)または推奨を意味するものではありません。

You’re now leaving st.com and will be re-directed to our Partner’s website.
For the latest innovations and solutions from ST, sign up for our newsletters.