Dracula Technologies, headquartered in Valence, France, pioneers sustainable energy solutions with their LAYER® technology, revolutionizing power sources for low-power electronics. Their Organic Photovoltaic (OPV) modules, manufactured using patented digital printing, harvest ambient light, eliminating reliance on traditional batteries.
LAYER® Vault complements their existing OPV harvesting product line, transforming it into a 2-in-1 product, combining low-light energy harvesting and storage on a single, flexible film ensuring uninterrupted device functionality, empowering Smart buildings, Smart homes, Smart asset tracking, and other related applications.
With a commitment to clean, renewable energy, Dracula Technologies leads the change towards a greener future by providing long-lasting, and cost-effective energy solutions.
Supporting their mission is their new "Green micropower factory"—a state-of-the-art, fully automated facility, the largest of its kind in Europe with a capacity of up to 150 million cm² of printed OPV devices per year.
Products of Dracula Technologies
Dracula Technologies offers two advanced energy harvesting solutions, both manufactured using state-of-the-art inkjet printing technology.
LAYER® is a flexible OPV module and LAYER® Vault combines an OPV layer and a supercapacitor on a single thin film ensuring both energy harvesting and storage. These energy solutions seamlessly integrate with low-power electronics, guaranteeing their full device autonomy.
LAYER® modules are distinguished by their thinness, flexibility, and adaptability. Thanks to inkjet printing, LAYER® enjoys a free-form design that can be integrated in any sensor size and shape. Operating even in extreme low-light environments, LAYER®’s performance is optimal in sub-500 LUX conditions and enables applications in the Smart Home & building and Smart asset tracking segments. Dracula Technologies has crafted a bespoke OPV module precisely suited to Semtech's application needs, specifically tailored for the STM32U0 microcontroller.
STM32U0 powered by LAYER®
Dracula Technologies’ LAYER® OPV technology was integrated into the STM32U0, granting it full energy autonomy thereby eliminating the need for traditional batteries. Even in challenging indoor low-light environments with as little as five LUX, equivalent to a very dim room, LAYER® continues to generate a sufficient amount of energy to ensure optimal device operation.
Leveraging the capabilities of Dracula Technologies' OPV, the STM32U0 achieves unprecedented static power consumption levels, empowering engineers to optimize their designs for a multitude of applications across industrial, medical, smart metering, and consumer wellness markets.
Dracula Technologies’ collaboration with STM32U0 thus opens the doors to applications that can excel with substantially smaller power sources.
Dracula Technologies in STMicroelectronics ecosystem
The collaboration between Dracula Technologies and STMicroelectronics represents a significant advancement for both companies, merging their expertise in low-power electronics to create autonomous energy solutions that meet market demands.
Dracula Technologies showcases the reliability of its technology in the low-power electronics segment by integrating its organic photovoltaic technology in STMicroelectronics microcontrollers. This synergy enables STMicroelectronics to elevate its products by making them fully energy-autonomous using Dracula Technologies' ambient light energy harvesting solution, LAYER®️, operating in low-light environments. By expanding its applications range, Dracula Technologies strengthens its position as a provider of sustainable and efficient energy solutions in the market.
For STMicroelectronics, this collaboration marks a new era of energy-efficient microcontroller units thanks to the access to expertise in organic photovoltaic technology and energy harvesting solutions. By integrating Dracula Technologies' know-how into its offerings, STMicroelectronics can now enable applications that demand ultralow power consumption, particularly crucial for numerous self-powered sensors relaying on energy harvesting instead of traditional batteries. This collaboration opens up new opportunities for STMicroelectronics to cater to a wider variety of applications and capitalize on the momentum towards sustainable technologies. The STM32U0 helps design teams to provide the optimal compromise between energy consumption, integrated features, and cost-effectiveness.
Dracula Technologies: Related Resources
Description | Category |
STM32U0 ULP Lux Demo | Video |

製品・サービス:
• コンパニオン・デバイス
• 開発ボード
所在地:
3 Rue Georges Auric, 26000, Valence, France
お問合せ先:
Jerome Vernet
ウェブサイト:
www.dracula-technologies.com
パートナー製品 | 概要 | 関連製品 | |
---|---|---|---|
Demokit | Free shape OPV module | STM32U0 series STM32U083C-DK |
パートナー製品 | 概要 | 関連製品 | |
---|---|---|---|
LAYER® | Organic photovoltaic (OPV) modules | STM32U0 series |
免責条項
本ウェブサイトで定める利用規約、ST販売取引条件およびプライバシー・ポリシーに加えて、次の条件がすべてのSTMicroelectronicsのパートナー・プログラムに適用されます。
STMicroelectronicsはウェブサイト上で正確な情報を提供することに務めています。しかし、STMicroelectronicsは、情報の正確性ついて一切の責任を負いません。本ウェブサイト上でSTMicroelectronicsが提供するすべての情報は、あらゆる欠陥を含んだ「現状有姿」のままで提供され、明示、黙示または法定のものかを問わずいかなる種類の保証もありません。STMicroelectronicsは、そのパートナー・プログラム、製品またはサービスを、予告なく、いつでも変更または停止することができます。STMicroelectronicsのものではない製品またはサービスに関する言及は専ら情報提供のためのもので、STMicroelectronicsによる推奨を意味するものではありません。本ウェブサイトにおける「パートナー」という言葉または用語の使用は、STMicroelectronics と他の企業との間にパートナーシップ関係、代理関係、法的関係もしくは信認関係が存在すること、あるいは当該企業が何らかの意味においてSTMicroelectronicsの関連会社であることを示すものではなく、またこれを示唆するものでもありません。STMicroelectronicsのパートナー・プログラムにおけるパートナーは、その製品および/またはサービスならびに関連技術をSTMicroelectronicsの製品と共に購入または使用することについて個別のライセンスを提供致します。ライセンス条件、価格、サポート、当該パートナーの製品および/またはサービスに関するその他の情報については、該当するパートナーに直接お問い合わせください。当該製品および/またはサービスに係る取引条件はパートナー毎に異なる場合があり、また当該パートナーから直接かつ個別にライセンスされます。STMicroelectronicsは、パートナーが提案または提供する製品およびサービスの適切性についていかなる表明も保証も致しません。STMicroelectronicsは、パートナーが提供する製品またはサービスについて、明示、黙示または法定のものを問わず、あらゆる保証および条件(商品性、特定目的の適合性、権原、非侵害の保証および条件、または取引、使用もしくは取引慣行から生ずる保証および条件を含みますがこれらに限りません)をここに否認致します。 STMicroelectronicsは、直接損害、間接損害、付随的損害、特別損害、懲罰的損害、結果損害またはその他のあらゆる損害について、たとえ当該損害の可能性について告知を受けていたとしても、如何なる場合も責任を負いません。かかる損害は原因の如何を問わないものであり、また契約、厳格責任、不法行為(過失またはそれ以外を含む)を問わずいかなる責任理論に基づくかを問わないものであり、またパートナー・プログラムへのお客様の参加・信頼、パートナーの製品および/またはサービスのお客様による使用、若しくはお客様がこれらを使用、購入できないこと、またはかかる製品およびサービスの性能、お客様とパートナーとの関係、STMicroelectronicsポータルまたは当該ポータルにおいてSTMicroelectronicsから提供される情報をお客様が使用すること、または使用できないこと、あるいは当該情報に対する信頼から生ずる、またはこれらに関連して生ずる使用、利益または収入の喪失を含みますが、これらに限るものでなく、損害発生の種類を問いません。STMicroelectronicsが提供するサードパーティーのウェブサイトへのリンクは、STMicroelectronicsの管理下になく、STMicroelectronicsは、リンク先のサイトまたはリンク先のサイトに含まれるリンクに在るコンテンツ、資料、意見、助言もしくは声明、また当該コンテンツおよび資料の正確性または信頼性、また当該サイトの変更もしくは更新について一切責任を負いません。STMicroelectronicsは、リンク先のサイトで受信するいかなる形式の通信(ウェブ放送または音声通信を含むがこれらに限らない)についても責任を負いません。リンク先のサイト、リン先のサイトに含まれるリンクへのアクセスはお客様ご自身のリスクで行ってください。STMicroelectronicsは、専ら便宜のためにお客様にこれらのリンクを提供しているものであり、リンクが含まれていても、STMicroelectronicsによるサードパーティーのウェブサイトの保証(明示、黙示、その他を問わない)または推奨を意味するものではありません。

You’re now leaving st.com and will be re-directed to our Partner’s website.
For the latest innovations and solutions from ST, sign up for our newsletters.