About Tuxera's HCC Embedded Brand
Tuxera develops deeply embedded software components “out of context”, which ensures that they can be used as core elements of any system, including those engineered to meet stringent requirements for safety, quality, and portability. Built on a foundation of quality, Tuxera has a product portfolio of more than 250 embedded components, with deep competencies in reliable flash memory management, fail-safe file systems, and IPv4/v6 networking stacks and their associated security protocols, as well as a comprehensive suite of USB host and function software. Since 2002, Tuxera has supplied these embedded software components to more than 2,000 companies globally in a wide range of industries including industrial, medical, and automotive.
Tuxera has built its organization on quality (ISO 9001:2015 and ISO 27001 certified) to deliver quality solutions.
With the introduction of its SEooC (Safety Elements out of Context), Tuxera is using its focus on developing reusable safety components to raise the standard of available embedded software elements even higher. The embedded world is changing rapidly in terms of the complexity of development environments and the complexity of the required solutions. Tuxera continues to evolve with this change and provides embedded solutions to help companies, across all industries and locations, meet these challenges.
Advanced Embedded Framework
Tuxera has developed more than 250 reusable software components for use in deeply embedded systems. To do this in a scalable way with consistent quality across these components, Tuxera has created its Advanced Embedded Framework (AEF), the standard to which all components are engineered. The AEF ensures that each component is independent from any particular architecture, RTOS, or toolchain. It also prescribes levels of quality to the code and its interfaces, to ensure that there is a consistent “look and feel” across the product range.
HCC Embedded products are used, without modification, in thousands of customer projects with over 30 different RTOSes, in 8, 16, 32 and 64-bit systems, big- or little-endian, with many architectures and tool chains.
Integrated Projects
Over the past 17 years, HCC has built more than 2,000 projects where HCC engineers have integrated HCC embedded components with its customers’ designs. The advantage of this approach is that Tuxera experts perform the software implementation on the customer-agreed target system. In this way, Tuxera provides its customers with a common platform for development and support. Customers are buying more than just software; they are engaging in a long-term engineering partnership.
#FuSa
製品・サービス:
• 組込み用ソフトウェア
所在地:
Vaci ut 76, H-1133, Budapest, Hungary
お問合せ先:
Contact
Company primary contact phone:
+36 1 450 2302
ウェブサイト:
www.hcc-embedded.com
パートナー製品 | 概要 | 関連製品 | |
---|---|---|---|
Tuxera Reliance Sense | Smart-meter File System (SMFS) custom-designed for smart energy & smart-meter applications | STM32 32-bit Arm Cortex MCUs | |
Tuxera IPSec/IKE | Security in embedded apps (cars, PoS, medical, industrial) | STM32 32-bit Arm Cortex MCUs | |
Tuxera Fail-safe File System | All Flash File Systems with fail-safe mechanisms for STM32 | STM32 32-bit Arm Cortex MCUs STM8 8-bit MCUs | |
Tuxera MISRA TCP/IPv4 and IPv6 | Embedded stack developed using a verifiable process and conforming strongly to MISRA coding standards | STM32 32-bit Arm Cortex MCUs | |
Tuxera TLS | Optimized software module designed to provide secure network communications | STM32 32-bit Arm Cortex MCUs | |
Tuxera USB Stack | USB Host & Device and OTG stacks with wide range of class drivers for STM32 | STM32 32-bit Arm Cortex MCUs | |
Tuxera SafeTCPIP | A complete TCP/IP v4 stack for safety-critical automotive, industrial, or medical embedded systems | STM32 32-bit Arm Cortex MCUs | |
Tuxera MQTT | MQTT is a small and efficient machine-to-machine protocol | STM32 32-bit Arm Cortex MCUs | |
Tuxera Bootloaders | Optimized high quality solutions bootloaders | STM32 32-bit Arm Cortex MCUs STM8 8-bit MCUs | |
Tuxera FAT File System | FAT File systems for flash storage media | STM32 32-bit Arm Cortex MCUs STM8 8-bit MCUs | |
Tuxera Embedded Encryption Manager (EEM) | Secure embedded systems using multiple encryption or hash algorithms through a uniform interface | STM32 32-bit Arm Cortex MCUs |
免責条項
本ウェブサイトで定める利用規約、ST販売取引条件およびプライバシー・ポリシーに加えて、次の条件がすべてのSTMicroelectronicsのパートナー・プログラムに適用されます。
STMicroelectronicsはウェブサイト上で正確な情報を提供することに務めています。しかし、STMicroelectronicsは、情報の正確性ついて一切の責任を負いません。本ウェブサイト上でSTMicroelectronicsが提供するすべての情報は、あらゆる欠陥を含んだ「現状有姿」のままで提供され、明示、黙示または法定のものかを問わずいかなる種類の保証もありません。STMicroelectronicsは、そのパートナー・プログラム、製品またはサービスを、予告なく、いつでも変更または停止することができます。STMicroelectronicsのものではない製品またはサービスに関する言及は専ら情報提供のためのもので、STMicroelectronicsによる推奨を意味するものではありません。本ウェブサイトにおける「パートナー」という言葉または用語の使用は、STMicroelectronics と他の企業との間にパートナーシップ関係、代理関係、法的関係もしくは信認関係が存在すること、あるいは当該企業が何らかの意味においてSTMicroelectronicsの関連会社であることを示すものではなく、またこれを示唆するものでもありません。STMicroelectronicsのパートナー・プログラムにおけるパートナーは、その製品および/またはサービスならびに関連技術をSTMicroelectronicsの製品と共に購入または使用することについて個別のライセンスを提供致します。ライセンス条件、価格、サポート、当該パートナーの製品および/またはサービスに関するその他の情報については、該当するパートナーに直接お問い合わせください。当該製品および/またはサービスに係る取引条件はパートナー毎に異なる場合があり、また当該パートナーから直接かつ個別にライセンスされます。STMicroelectronicsは、パートナーが提案または提供する製品およびサービスの適切性についていかなる表明も保証も致しません。STMicroelectronicsは、パートナーが提供する製品またはサービスについて、明示、黙示または法定のものを問わず、あらゆる保証および条件(商品性、特定目的の適合性、権原、非侵害の保証および条件、または取引、使用もしくは取引慣行から生ずる保証および条件を含みますがこれらに限りません)をここに否認致します。 STMicroelectronicsは、直接損害、間接損害、付随的損害、特別損害、懲罰的損害、結果損害またはその他のあらゆる損害について、たとえ当該損害の可能性について告知を受けていたとしても、如何なる場合も責任を負いません。かかる損害は原因の如何を問わないものであり、また契約、厳格責任、不法行為(過失またはそれ以外を含む)を問わずいかなる責任理論に基づくかを問わないものであり、またパートナー・プログラムへのお客様の参加・信頼、パートナーの製品および/またはサービスのお客様による使用、若しくはお客様がこれらを使用、購入できないこと、またはかかる製品およびサービスの性能、お客様とパートナーとの関係、STMicroelectronicsポータルまたは当該ポータルにおいてSTMicroelectronicsから提供される情報をお客様が使用すること、または使用できないこと、あるいは当該情報に対する信頼から生ずる、またはこれらに関連して生ずる使用、利益または収入の喪失を含みますが、これらに限るものでなく、損害発生の種類を問いません。STMicroelectronicsが提供するサードパーティーのウェブサイトへのリンクは、STMicroelectronicsの管理下になく、STMicroelectronicsは、リンク先のサイトまたはリンク先のサイトに含まれるリンクに在るコンテンツ、資料、意見、助言もしくは声明、また当該コンテンツおよび資料の正確性または信頼性、また当該サイトの変更もしくは更新について一切責任を負いません。STMicroelectronicsは、リンク先のサイトで受信するいかなる形式の通信(ウェブ放送または音声通信を含むがこれらに限らない)についても責任を負いません。リンク先のサイト、リン先のサイトに含まれるリンクへのアクセスはお客様ご自身のリスクで行ってください。STMicroelectronicsは、専ら便宜のためにお客様にこれらのリンクを提供しているものであり、リンクが含まれていても、STMicroelectronicsによるサードパーティーのウェブサイトの保証(明示、黙示、その他を問わない)または推奨を意味するものではありません。

You’re now leaving st.com and will be re-directed to our Partner’s website.
For the latest innovations and solutions from ST, sign up for our newsletters.